[ DRV8303 ] Bootstrap Diode Characteristics
Hi,
Can you please let me know the characteristics of internal bootstrap diode?
Min | Typ | Max | Unit | Note | |
Forward Voltage | [ V ] | ||||
Forward Current | [ mA ] | ||||
Resistance | Ohm |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please let me know the characteristics of internal bootstrap diode?
Min | Typ | Max | Unit | Note | |
Forward Voltage | [ V ] | ||||
Forward Current | [ mA ] | ||||
Resistance | Ohm |
Hi Ken,
What is reason for understanding these parameters? This will help us to better answer this request.
Ken,
Do you know what the part number is for the device these parameters are from?
I am trying to understand the test conditions. Do you know why these specific test conditions are selected?
Hi Phil,
Thank you for sharing information!
You don't have intention to specify this in the datasheet, correct?
Min | Typ | Max | Unit | ||
Forward Voltage Vf | IF=0.5mA | 0.676 | 0.85 | V | |
Forward Current If | Vf=1V | 100 | 500 | 1600 | mA |
Diode Resistance | Vf1=0.95V, Vf2=1.05V | 170 | 320 | 680 | mohm |
Sorry, let me ask one more thing.
What is the min, typ and max of trickle charge current?
Min | Typ | Max | Unit | Note | |
Trickle Charge Current |
Thanks,
Ken
Ken,
MAX output capability is 20 uA. The majority of this output capability is used to support internal leakage paths. If 100% operation is required we recommend keeping the resistance >1MOhm between the gate and source pins of the external MOSFETs.
There is no plan to update the datasheet with these values.