Part Number: DRV8834
Other Parts Discussed in Thread: DRV8880
I am attempting to drive a small stepper motor with the DRV8834. This motor has a 48 Ohm winding resistance and is intended to be operated at 4V. The peak current should be less than 100mA. We are micro stepping at 8x and see little motion for the micro steps then a big jump at the full step boundary. When I look at the current to the motor winding it goes to zero during each PWM cycle, regardless of step. If I could reduce fixed off time I assume the PWM might turn on again before the current goes to zero. Is there a more suitable driver for this small motor? I am looking at the DRV8880 and am intrigued by the Tourque DAC setting, is this a way to configure the IC to drive a smaller motor? Sorry but I do not know the winding inductance or the degrees per step for this motor. I am working from a rather weak stepper driven iris datasheet that I will attach.VP-9610(www) specification (optoskand151023 hunter170726).pdf