Other Parts Discussed in Thread: DRV8837,
Dears:
We are checking the performance between DRV8839 and DRV8837.
Could you give some advice about the below questions:
1. DRV8837 has two braking mode when it controls two motors, and do DRV8839 have braking mode?
Do DRV8839 happen the phenomenon of mixed braking mode if DRV8839 is driving two motors at the same time (the PWM of the two motors is independent and independent).
2. Is there any diagrams about Forward Direction and Reverse of 50% ,20% Duty Cycle?
3. Is the different between DRV8839 controlling one Motor and DRV8839 controlling two Motors from the Motors' power, response time, braking mode etc?
Thanks a lot!
Best regards
Luck Wu