Part Number: DRV8818
HiI
read the following post. However I have some question about a capacitor for connecting to the pin.
1. Are there any recommended value range for CP1-CP2 and VCP and VGD?
Our customer would like to consist that capacitor by a few (0.1uFx 2~3) parallel capacitor. (0.2~0.3uF is possible?) How much Is the range possible?
(Please let me know if there is any other concerns.)
2. If those capacitor is too small or too large, what is affected to the operation?
3. How much is the maximum voltage will biased at CP1-CP2 and VCP and VGD pin?
Our customer would like to consider the maximum biased voltage for the capacitor at those pins.
I saw the EVM BOM. The capacitor are used 50V capacitor. (C0805C224K5RACTU)
Should we use the 50V capacitor same as EVM? Or is it possible to use a capacitor less than 50V? (Supply Voltage : 24V +/-10%)
Best Regards,
Koji Hamamoto