Other Parts Discussed in Thread: DRV2700, DRV2700EVM-HV500
Hello,
I am using the DRV2667 as a voltage-controlled source to create the waveform below. I have the driver programmed to 50Vpp (Gain 01 with recommended resistors) with a boost current limit of 1.8A (Rext = 7.87kohm). Each output trace contains a 600ohm ferrite bead and a 100ohm resistor. When I set the output to the maximum intensity using a 1000ohm load, I get a Vpp of ~72v, but the signal is degraded. The rms current at this intensity is about 18mA. Is the current saturating to cause the distortion? How can I stop the distortion of the signal? Is there a way to boost the output rms current to 40mA?
Thank you!