Part Number: DRV120
Other Parts Discussed in Thread: DRV110
What would be the maximum output (solenoid) current for this device. I am anticipating my application will require .250-.300A, for peek, with significantly less for hold.
Thanks!
Hank Z.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hank,
Let me contact the expert for this part. You can expect a response by 10/21/19 (edited from 10/19/19 since it is on a weekend).
Best,
Grant
Hi Hank,
DRV120 max peak current is 250mA. To get the max current Rpeak=50kohm
For higher peak current, recommended device is DRV110. It is similar to DRV120. The FET is extrenal, allowing a wide range of Ipeak and Ihold
Regards,
Costin