Other Parts Discussed in Thread: DRV8412
Hello Support team,
My customer is investigating DRV8801-Q1 for non motor application. They request us to review if DRV8801-Q1 can support their usage. Could you support?
They plan to control Phase, MODE1 and MODE2 by PWM signal
MODE1: 100kHz to 120kHz
MODE2, PHASE: 50kHz to 60kHz.
Need to control OUT A/B separately
Especially, they would like to control MODE1 with up to 120kHz. Can DRV8801-Q1 support this? PHASE and Enable is recommended to use below 100kHz, however, there is no information for MODE1 fPWM on datasheet.
If DRV8801-Q1 can't support, could you tell me your recommended device?
Thanks,
Koji Ikeda