This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983-Q1: Load transient immunity

Part Number: DRV10983-Q1
Other Parts Discussed in Thread: DRV10983,

Hi Team,

I can see the Vin spec which is like VCC during load dump (VCC slew rate < 1 V/µs) –0.3 45V on the datasheet.

In this case, is it meets the ISO16750(http://www.compel.ru/wordpress/wp-content/uploads/2017/05/ISO-16750-22010E-.pdf)?

If customer's the battery meets ISO16750, DRV10983 can also meet the load dump criteria. Is it correct?

Thanks,

Uchihara