This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2667: problem with ripples on VDD input

Part Number: DRV2667

Hi,

I'm driving the DRV2667 with a 5V-supply. While generating a sinusoidal signal on the output I'm generating quite big ripples on the 5V supply. Is this a known problem or is it based on errors in the circuit design? Prbably someone has an idea where they come from an how to get rid of them? I use 100nF capacitors close to VDD pin and on the supply side of the inductor which is connected to SW pin (see below).

I appreciate your help!

Best regards

Dietmar