Part Number: DRV8353
Hi Team,
For the VDS or VSENSE over-current protection of DRV8353, the customer chooses the CBC mode. Is it necessary to have the rising edge of INH or INL of the phase where the over-current is detected when recovering? Or for all 6 inputs, as long as there is a rising edge, it will be reset and the output can be restored?
In addition, will this be related to the setting of OCP_ACT?
If he uses 1x PMW mode, is it to restore output through INHA? Will it affect the Hall signal input number?
Thanks,
Annie