Hi Team,
I understand that Parity bit is “Error detection code bit”.
-SPI_PARITY resister is 0x0, No SPI parity error is detected
-SPI_PARITY resister is 0x1, SPI parity error is detected
Could you please let us know the behavior or Parity bit at the following condition?
-If SPI_PARITY resister is 0x0, Parity bit is “0” or “1” or “Indefinite”.
-If SPI_PARITY resister is 0x1 and data bit "1" is even, Parity bit is “0” or “1”.
-If SPI_PARITY resister is 0x1 and data bit "1" is odd, Parity bit is “0” or “1”.
Regards,
Hide