Dear team:
One of my customers changed the MOSFET pre-driver chip and op amp chip on the basis of BOOSTXL-DRV8305EVM. When running the lab_02b program, the current will be very large and the motor will also be stuck. So he has the following questions:
1, The op amp he used in his circuit board design is a positive feedback op amp, so besides modifying the void HAL_updateAdcBias function in the code, which function needs to be modified? How to modify?
2, In addition to modifying the positive and negative feedback of the op amp, the op amp multiple, and the voltage feedback, what parameters need to be modified in the software?
Best regards