Other Parts Discussed in Thread: BQ32000
Hi folks,
I am using BQ32000 RTC in my design.battery is fully discharged after came from assembly house.3V battery is discharged to 0.6V within 4 days or less.I observed same this condition in all the boards.
We observed below strange behavior i.e; I connected current meter in series to battery to monitor the current.
That time my board is in turnoff and only monitoring the battery discharging current.
As per datasheet(page no. 4 I backup supply current) ,it should not take discharge current more than 1.5uA.But sometimes it is taking 60uA of discharging current(whenever i am trying connect the multimeter operating in current mode) and sometimes 1.9uA of current.
If issue will be the probing, then it should give 21 days battery backup .I am not able to conclude that what might be the issue.I opened ground pin of RTC(suspected leakage current) and connected battery directly on RTC 3rd and 4th pin.I observed the still same behavior.
We assembled only RTC IC and battery(MS412FE-FL26E) on the bare PCB board and observed battery discharging current, the behavior is same as above mentioned.
I did one more experiment , i added schottky diode from battery to IC 3rd pin.Still I observed the same problem as above.
I have added series 10K resistor instead of diode from battery to RTC 3rd pin.Constant voltage drop 19.3mV observed across resistor.
I have attached my RTC circuit for reference.Initially C90 and C94 are mounted on the board,while testing we removed the capacitors.
The above mentioned details are the our observations.We used rechargeable battery instead of non-rechargeable battery.
Please some body suggest me regarding this issue.
Thanks in advance.
Regards
Swapna.B