Other Parts Discussed in Thread: DRV8301
Using DRV8301 in our product, we are trying to intentionally trigger faults on DRV8301 and we are seeing some misbehavior from the chip:
- Under load, the supply voltage drops significantly intentionally to create fault. These should trigger two kind of faults:
- MOSFET short circuit: this is becaus eteh low supply would result in MOSFETs not turning on properly and show large VDS
- Low supply voltage
- We have set the fault to OC latch mode
- We can get these faults to happen, but although the driver stops momentarily, mostly the fault is not latched. That's the first bad behavior
- Sometimes the fault is latched, but only showed fault, and no OC condition. This could be because we continuously read the register
. This should be normal
- When the fault latches, we cannot reset the chip by toggling EN_GATE pin. This is the second issue.
Will you please tell me why we would have such behavior? Thanks.