In the TL431 datasheet (SLVS543M) there is a test circuit to measure the Reference Impedance.
Can anybody explain how that measurements works? I miss the ac coupling...
Thanks for any suggestion.
Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the TL431 datasheet (SLVS543M) there is a test circuit to measure the Reference Impedance.
Can anybody explain how that measurements works? I miss the ac coupling...
Thanks for any suggestion.
Chris
Christian,
AC coupling is not needed here becuase VIN[dc] is 0V.
The circuit works fine for simulation, but it not the most practical setup in reality.
The 50 resistor is pointless because the simulated AC generator has zero impedance; a real source will likely be 50 ohm internal. The voltage source (set to get required cathode current) is also simulated as zero impedance, a real supply would be a complex impedance, so bypass caps (plural) are highly recommended.
The basic theory is that the 1k resistor and the TL431 impedance form a voltage divider. The AC voltage on the TL431 vs. the input AC voltage and 1k fixed resistor is mathematically converted into TL431 impedance value.