Part Number: BQ27750
Other Parts Discussed in Thread: BQSTUDIO
Hey,
I'm working on BQ27750 single cell unit in my project and facing some following issue:
1. Communicate the BQ27750 with PSOC 4 micro controller via I2C, when Load is connected DFET and CFET is on after some threshold DFET gets off but still some negative current is shown and battery still get discharge with slow rate. (command is ( 0xAA + 0x3E + 0x20 + 0x00 ) for DFET & for CFET ( 0xAA + 0x3E + 0x1F + 0x00 )).
2. On Every reset the BQ27750 go into the sealed mode. Please tell me the Command of Unseal mode or full access mode and how to write via I2C.
3. On reading Operation_Status Register, it show that BQ27750 is in Reserved mode but I unable to write the register like Shutdown Threshold, Sleep Threshold etc.
Regards
Rahul Kumar
rahul1.kumar@vnl.in
8860719701