Hi,
TPS63020-Q1's datasheet describes 2 kinds of VFB spec in P.5, one is at PS/SYNC = VIN and the another one is at PS/SYNC = GND.
Why are the specs defined separately? PLS tell me the reason to separate and the reason why the VFB spec at PS/SYNC = GND has wider range.
PLS also tell me the reason why the VFB at PS/SYNC defined with using percentage, -0.6% of 500mV for min and +5% of 500mV in max.
Best Regards, Taki