Other Parts Discussed in Thread: TPS630250,
Dear Team,
Our customer follow the EVB schematic, but the voltage get big ripple around 500mV.
Could you guide us how to check it?
Thanks a lot!
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Can you share the schematic and layout? We will need to take a look to do further debug.
What kind of scope probe are they using for measurement?
Sincerely,
Wyatt Keller
Hi Keller,
We appreciated your great support!
The schematic and Layout as below for your reference.
Many Thanks,
Jimmy
Hello Jimmy,
It looks like the ripple is very low frequency, do you have your system attached during the test? It may be due to the system load and not the charger. This is not from the switching ripple. Can you also capture waveforms of the battery current/voltage along with the bus current/voltage?
The layout and schematic look okay from what I can see.
Sincerely,
Wyatt Keller
Hi Wyatt,
We appreciated your great support!
Customer have a question as below:
Why the TPS25619 need to consume that much current to keep waveform smooth ?
(waveform)
1.No load :TPS25619 have 15Hz ripple
TPS630250 -> perfect
2.33 ohm resister load :120mA
TPS25619 have 15Hz ripple
TPS630250 perfect
3.10 ohm load:420mA
TPS25619 perfect
TPS630250 perfect
Best regards,
Jimmy
Hello Jimmy,
Can you share your registers settings and your system specs (input voltage, input current, charge current)? Are you measuring the ripple on the system of bat pin?
Also just to clarify you're still wondering about the bq25619? I won't be familiar with the TPS chipset.
Sincerely,
Wyatt Keller
Hi Wyatt,
Thanks for your support!
I have checked it with our customer:
1. They don't set the register .
2. They don't connect the battery , and they check the voltage that is from vout.
Could you help to why the TPS25619 need to consume that much current to keep waveform smooth ?
Many Thanks,
Jimmy
Hello Jimmy,
So they use all default register values?
They don't connect the battery during this test or the measurement is not on the battery? Do they see the voltage ripple on VSYS? Can you share scope captures of VBUS, VSYS, VBAT, and VSYS?
Sincerely,
Wyatt Keller