This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Is that possible to test the fast charging of bq25792 using USB-PD-CHG-EVM-01 ?

Part Number: BQ25792
Other Parts Discussed in Thread: TPS25750, , USB-PD-CHG-EVM-01,

Hi,

I am using bq25792 along with tps25750 USB Type C PD controller. I am planning to develop a power bank.

For the same I am planning to test Fast charging using this combination (tps25750 + bq25792). For the same I am using " USB-PD-CHG-EVM-01 evaluation module (EVM) ".

From the datasheet of BQ25792 I found that it support fast charging and from the datasheet I found this below sentence. 

"To support fast charging using adjustable high voltage adapter (HVDCP), the device provides D+/D- handshake."

But when I checked the schematics of USB-PD-CHG-EVM-01 the USB lines of BQ25792 is unconnected as shown in the below image.

So, is that possible to check the Fast charging using USB-PD-CHG-EVM-01 evaluation module .