Other Parts Discussed in Thread: TPS25750, , USB-PD-CHG-EVM-01,
Hi,
I am using bq25792 along with tps25750 USB Type C PD controller. I am planning to develop a power bank.
For the same I am planning to test Fast charging using this combination (tps25750 + bq25792). For the same I am using " USB-PD-CHG-EVM-01 evaluation module (EVM) ".
From the datasheet of BQ25792 I found that it support fast charging and from the datasheet I found this below sentence.
"To support fast charging using adjustable high voltage adapter (HVDCP), the device provides D+/D- handshake."
But when I checked the schematics of USB-PD-CHG-EVM-01 the USB lines of BQ25792 is unconnected as shown in the below image.
So, is that possible to check the Fast charging using USB-PD-CHG-EVM-01 evaluation module .