Other Parts Discussed in Thread: TPS28225,
Hello,
I'm Anesh working from Robert Bosch India. My contact number is +919003779933.
For one of our development project to drive 3 phase PMSM machine we need Automotive graded Half Bridge Gate driver with Single PWM input (Input H and L with inverted logic), Enable/Shutdown input.
For example device like TPS28225 to drive Half bridge MOSFET with large input capacitance power MOSFETs. Operating voltage must start from 6V.
Or a B6 Bridge driver without SPI interface. We will not have microcontroller on board. We will receive just 3 PWM inputs from another unit.
Please suggest me some devices.
Thanks, Anesh S.