Part Number: TPS563202
Hi team,
I see that the control mode of TPS563202 is D-CAP2, but according to 7.3.1 Adaptive On-Time Control and PWM Operation, this control mode is like COT mode.
I think the D-CAP2 mode should be as follows.

Another question is the on-timer. This one shot duration is set proportional to the converter input voltage, VIN, and inversely proportional to the output voltage, VO, to maintain a pseudo-fixed frequency over the input voltage range. I think on duration should be inversely proportional to the converter input voltage, VIN, and proportional to the output voltage, VO. What do you think?
Br,
Nison