Hi,
I set the OCC Threshold to 4mV (in my case is 2.1A), the delay to 3.3ms, the Recovery Threshold to 600mA and the PACK-TOS Delta 100mV (Stack Voltage = 57.02V and TOS Voltage = 3.656V).
The protection triggers correctly and opens the mosfets. I don't understand why the error disappears and closes the mosfets with the recovery delay (5s) after reducing slightly the charge current without having reached the recovery threshold. Is there any other recovery condition other than the Threshold or the PACK-TOS Delta?
Thank you in advance!
Mohamed