Part Number: UCC27289
Other Parts Discussed in Thread: UCC27714
Hi,
Can the UCC27289 use on the two switches topology?
There has another power for the HB pin, and the switch turns on together.

thanks and best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rock,
Regards,
Hi Richard
Can UCC27289 use the same circuit as UCC27714 datasheet Figure 49? My customer has PCB size considerations.
And could you also explain the operation principle of the datasheet Figure 49, thanks
Regards
Rock
Hello Rock,
The circuit in the UCC27714 can be used, the boot diode shown in the diagram would not be installed, as the UCC27289 has an internal boot diode.
The principle is the driver low side output when turned off turns off the aux transistor (bottom switch) which allows the aux transistor top switch to turn on. The aux switch (top) turning on provides a path for the driver HS to be pulled to ground which provides a charging path for the bootstrap capacitor to charge from VDD through the boot diode.
During the power switch off time, the HS is pulled low allowing the boot cap to charge.
Regards,