Dear Team ,
Good day!
Our customer are trying to use the TPS546D24A , but he do not prepare to use the PMBUS , they want to fix the output voltage /frequency /UV /OV by hardware , as the datasheet mentioned that
"The Hardware for VOUT_OV_FAULT_LIMIT is implemented as a fixed percentage of the current output voltage target"
For the output voltage and frequency , I think it will be fine via hardware setting , but for the UV / OV , the datasheet just describe the hardware can fix the percentage , but do not describe which pin determined
the value , it do not have the value map neither .
So , My query is :
Does the TPS546D24A support use the hardware setting to modify the " VOUT_OV_FAULT_LIMIT ” “VOUT_OV_FAULT_RESPONSE” “VOUT_OV_WARN_LIMIT” (40h-45h), without PMBUS .
BR,
Leon.liu