Other Parts Discussed in Thread: BQ34Z100, GPCCHEM
I'm trying to fine-tune the settings for a new battery pack. After letting the system discharge overnight, it was down to
13.164 volts FCC=15.014 RC=11.222 SoC=75%
I then power-cycled the unit, which restarted the BQ34Z100-G1 too. The new reported data from the part was
13.192 volts FCC=15.072 RC=9.458 SoC=63%
I cannot keep the BQ34Z100 from being power-cycled, due to the way the hardware is setup.
Which Data Flash settings would be most applicable to trying to get the part to make more consistent initial estimates?
(If I am at XX% and I power-cycle, I would like it to be at least close to XX% when it comes back up).