There is a question about the Output Voltage of the UCC28089 OUTA/OUTB. In the below condition, the VOL and VOH level is about 0.5 to 1V at 9Vdd. if this is a case, how does it drive the ext. MOSFET?
In customer condition, the VDD is 15V, what about the output voltage Level?
application: AC Motor Inverter
Usage: Bias power of the Gate driver
====================================================================================================
TA = --40°C to 105°C for UCC28089, VDD = 9 V (see Note 1), 1 μF capacitor from VDD to GND, RA = 110 kΩ, RB = 182 Ω, CT = 220 pF, TA = TJ,
VOL (OUTA or OUTB) IOUT = 75 mA =>0.5V(typ)1 V(max)
VOH (OUTA or OUTB) IOUT = --35 mA (VDD – VOUT) => 1.0(typ) 1.3(max)