Other Parts Discussed in Thread: TLV713P-Q1, TLV733P-Q1, TPS784-Q1
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "S-19252A18H-N4T1U4" ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "S-19252A18H-N4T1U4" ?
Hi Kygo,
We do not have an automotive LDO in the SC82 package, but we do have several options which matchup well with the S-19252 in the SOT23 package.
TLV713P-Q1 | TLV733P-Q1 | TPS784-Q1 | |
AEC Q100 | YES | YES | YES |
Output Options | Fixed Output | Fixed Output | Adjustable Output, Fixed Output |
Iout (Max) (A) | 0.15 | 0.3 | 0.3 |
Vin (Max) (V) | 5.5 | 5.5 | 6 |
Vin (Min) (V) | 1.4 | 1.4 | 1.65 |
Vout (Max) (V) | 3.3 | 3.3 | 5.5 |
Vout (Min) (V) | 1 | 1 | 1.2 |
Fixed Output Options (V) | 1, 1.2, 1.8, 2.5, 3.3 | 1, 1.1, 1.2, 1.5, 1.8, 2.5, 2.8, 3, 3.3 | 0.8, 1.2, 1.5, 1.7, 1.8, 2.5, 2.8, 2.9, 3, 3.3, 5 |
Enable | YES | YES | YES |
Power Good | NO | NO | NO |
Output Capacitor Type | Cap Free, Ceramic | Cap Free, Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 17 | 28 | 45 |
Noise (uVrms) | 55 | 120 | 30 |
Accuracy (%) | 1.5 | 1.4 | 1.5 |
Vdo (Typ) (mV) | 230 | 125 | 200 |
Iq (Typ) (mA) | 0.05 | 0.034 | 0.033 |
Thermal Resistance θJA (°C/W) | 249 | 93 | 171 |
Min Package Area (mm2) | 4.64 | 4 | 4.64 |
Package Type | SOT-23 | SOT-23, WSON | SON, SOT-23 |