Other Parts Discussed in Thread: UCC28600
Hi Team,
in led display application, do we have fly-back ACDC solution?(Size optimized solution)
the input need to tolerance 1000 surge test. Input is 220V narrow voltage.
12V output, peak 4.5A, normal 4A.
in led display application, the current is lower than 2A.
any mature solution we have?
thanks a lot.(In addition, about this case, do we need much bandwidth to do support? or this is mature solution, we can handle it by many documents we have.)