Other Parts Discussed in Thread: EV2400, BQ40Z50
Hello,
We are developing a product with a BQ27421-G1 fuel gauge. I have used Battery Studio along with the EV2400 USB to i2c inteface to set the correct parameters for the fuel gauge, and I then clicked on "Save to Gauge" to write these parameters onto the gauge.
1. Will this be written in the gauge non-volatile memory?
2. Is this actually enough for the gauge to provide me with accurate data? Or do I also need to execute a "Learning cycle"?
3. If the above is yes, will I be able to extract the data fro the learning cycle and flash it into the memory when I get to mass production?
Thanks