This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: Learning Cycle necessary?

Part Number: BQ27421-G1
Other Parts Discussed in Thread: EV2400, BQ40Z50

Hello,

We are developing a product with a BQ27421-G1 fuel gauge. I have used Battery Studio along with the EV2400 USB to i2c inteface to set the correct parameters for the fuel gauge, and I then clicked on "Save to Gauge" to write these parameters onto the gauge.

1. Will this be written in the gauge non-volatile memory?

2. Is this actually enough for the gauge to provide me with accurate data? Or do I also need to execute a "Learning cycle"?

3. If the above is yes, will I be able to extract the data fro the learning cycle and flash it into the memory when I get to mass production?

Thanks