Other Parts Discussed in Thread: LMZ31506, LMZ31707
We use these Texas Instruments DC-DC converters in multiple designs. The PTH12050W is used to convert 12V down to both 3.3V and 1.2V.
Issue we are seeing is that the modules that convert down to 3.3V run very hot to the touch. Touching the magnetics can burn, while the other 1.2V does not.
The 3.3V converter is very lightly loaded, less than 100mA maximum compared with the 1.2V which uses 2A. The datasheet does not specify a minimum load requirement. The converters work fine, why the drastic difference in their temperature? Heat is not good for magnetics.