Other Parts Discussed in Thread: BQ24040, BQ25170
I have a prototype here with LM3658. The application looks the same as the typical application in the datasheets. Right now there is a protection circuit on the battery that shuts off the voltage output below 2.8V. So the system sees "no battery". If I connect 5V to CHG_IN on LM3658 I only have about 1.5V on BATT from LM3658. I guess it's a problem for the circuit if it does not see a battery. However, can one in any way force the circuit to emit a charging voltage after the battery shuts off internally?