This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UA78: Search UA78 but need TO-252(DPAK)

Part Number: UA78
Other Parts Discussed in Thread: LM317

Hi Team,

There is good news that we DIN UA7805CKTTR

But now customer need TO-252(DPAK) package 

Do we have the solution

  • Kygo,

    LM317AMDTX/NOPB will be the best option, but it will be a adjustable version.

      UA78 LM317
    AEC Q100 NO NO
    Output Options Fixed Output Adjustable Output
    Iout (Max) (A) 1.5 1.5
    Vin (Max) (V) 38 40
    Vin (Min) (V) 7 3
    Vout (Max) (V) 24 37
    Vout (Min) (V) 5 1.25
    Fixed Output Options (V) 5, 8, 10, 12, 15, 24 -
    Enable NO NO
    Power Good NO NO
    Output Capacitor Type Cap Free, Non-Ceramic Non-Ceramic
    PSRR @ 100KHz (dB) 40 38
    Noise (uVrms) 52 38
    Accuracy (%) 3.75 5
    Vdo (Typ) (mV) 2000 2000
    Iq (Typ) (mA) 4.3 5
    Thermal Resistance θJA (°C/W) 22 24
    Min Package Area (mm2) 87.2744 45.5
    Package Type DDPAK/TO-263, TO-220, TO-220

    DDPAK/TO-263, SOT-223, TO-252, TO-220

    Regards,

    Prakash L