Other Parts Discussed in Thread: TPS61022
Hi,
I need to design 5 V power supply with Li-ion battery. So, input parameters are Vin= 2.8~4.2 V, and output parameters needs to be Vout=5V and Iout=3.5 A. I intend to use TPS61023 with valley current limit of 3.7 A. I was researching the term of valley current limit on TI forum and came up to conclusion that it can handle 3.5 A output current. This is my design below.
Is my conclusion about TPS61023 output current correct? What is maximum current it can give to output? Will this design work for my output needs?
And also, if I got this wrong, please explain what valley current limit means. Suggestions for design are welcome of course.
Thank you.