Part Number: TPS43000
Other Parts Discussed in Thread: TINA-TI
Hello,
I have been using the TPS43000 in a ZETA DC/DC converter with a good results since 2017, using a network experimentally derived from the SEPIC circuit in the data sheet. To be noticed that we use the PFM with DCM, so the regulation should obtain some benefits from this configuration.
Recently, I have dived deeper in the compensator network to optimize as most as possible the behavior against transients increasing the bandwidth; in the data sheet I have found a unit gain bandwidth of 5 MHz and assumed a A0 gain of 1000 for the internal feedback OPAMP.
Now, going to the point, essentially, increasing the bandwidth means to increase the gain but we have met some problem of stability at certain levels of gains: it seems that with gains higher than 20 dB between poles and/or higher than 0 dB between zeroes, the PFM is held also at output current values where it should not, like the output of OPAMP (internal at TPS43000) will be in someway saturated!
Having a look at the reference circuits in the data sheet SLUS489 − OCTOBER 2001, I have noticed that the gains in the compensator networks proposed are really low:
- the maximum gain between poles is +11 dB for SEPIC topology
- and between zeroes is -4.5 dB in the BUCK topology.
At this point, I do think that should be a limits in the gains due some parameters, I may suppose they are the maximum compensator output voltage (or modulator ramp voltage) and the regulation drift (in PFM is the 2% of Vout). But all those are speculations, then I'd like to know something more to obtain the maximum from the circuit I have designed.
Of course, it might be that everything above is wrong.... then tell me, please!
Thanks a lot for helping me.
Maurizio