Other Parts Discussed in Thread: BQ40Z50, , BQ76920, BQ78350
Hi there,
I am looking for a BMS-IC that can handle 4 LiFePo cells (4s1p) with a total capacitiy up to 180Ah with CC and DCC up to 180A. Active balancing is mandatory as well as SOC and SOH (via I2C/SMB/SPI/... interface).
I came across the BQ78PL114S12 which seems to a nearly perfect fit, except for the current range of 110A which is stated in the datasheet's front page. We need the ability of discharge of 180A for at least 10 minutes while maintaining correct SOC readings.
So bascially I am looking for a IC or combination of ICs (might be a gas-gauge + protection IC for SOC+SOH plus additional ICs for active balancing) for LiFePo chemistry.
Is it suitable to use active balancing ICs in addition to a passivly balancing BMS-IC?
Thank you very much
Karl