This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521825: LP873347 and TPS6521825: Will either PMIC cause voltage spikes when shutting down?

Part Number: TPS6521825

Hello,

I am considering using the LP873347 and TPS6521825 to power an i.MX 8M Mini processor. A previous PMIC I was evaluating for this purpose has the weird quirk where, when the PMIC was commanded to turn off, it would cause a spike on the input voltage rail (the rail supplying power to the PMIC). I wrote about this issue here: https://community.nxp.com/t5/Power-Management/PF8200-VIN-spikes-when-shutting-down/m-p/1251606. I'm also attaching an oscilloscope screenshot of the issue.

This "quirk" has caused me a number of headaches, so before I choose a new PMIC, I figured I should ask: Do either the LP873347 or TPS6521825 exhibit any behavior like this? Are there any situations where commanding either PMIC to turn off will backfeed current into the input voltage rail? Or cause a voltage spike on the input voltage rail? 

Thanks