Other Parts Discussed in Thread: EV2400
Hello,
We are using BQ27441 in low-power devise, the battery capacity is 500mAh, the min consumption around 10 mA, the max consumption around 1000mA
Using GPOUT Pin as SOC_INT. Getting the interrupt for Change in SOC. Also getting the interrupt for charge state change. But no interrupt for discharge state.
Tried to configure below registers but no results:
Dsg Current Threshold
Chg Current Threshold
Quit Current
Equation to calculate bit confusing to me.
The discharge current threshold can be calculated as Design Capacity / (Dsg Current Threshold × 0.1).
Seems are related SOC_INT issue [DSG flag bit] & Configuration of Threshold registers. Any related input will be helpful.
Thanks
Zahir