Hi team,
there is a conflict of BIT11 and BIT1. Are these bits read only of R/W? Does write these bits will take effect?
If the IC is be at boost mode, BIT1 is set to 1 and then write 0 to this bit frequently, what will happen?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
there is a conflict of BIT11 and BIT1. Are these bits read only of R/W? Does write these bits will take effect?
If the IC is be at boost mode, BIT1 is set to 1 and then write 0 to this bit frequently, what will happen?
Hi Allen,
Sorry for the confusion. These bits are read-only, so it is not possible to write to these bits and change their value. Figure 12 should label these bits as R, not R/W.
Best regards,
Angelo