Part Number: UCC5870QDWJEVM-026
Hello Guys,
Good day.
Thanks and regards,
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC5870QDWJEVM-026
Hello Guys,
Good day.
Our customer have clarification regarding the output voltage of UCC5870QDWJEVM-026.
In the datasheet it says: Driver output voltages by default are +15V/-8V with 12-V input supply.
For IGBTs customer will need +15V/-10V and for SiC Mosfets +20V/-5V. How can they adjust the output voltage of the evaluation board to meet this?
Thanks and regards,
Art
Hi Art,
The isolated bias power supply on the EVM is designed for +15/-8V only. For the low side driver, customer has the option to connect external power supply for VCC2, VEE2 directly(not connecting the 12V power supply). But this will be for low side only. If customer wants to use both high side and low side drivers with a different VCC2/VEE2 voltage, a transformer with different turns ratio will be needed for T1 and T2.
Regards,
Gangyao