I'm using TLV767 to actually make a board and drive LEDs.
TLV767 is a type with fixed 3.3V output
There is no problem until the input voltage is around 5-9V.
When it becomes 9V or more, it will oscillate around 3.3V.
The amplitude of oscillation is about 1V.