Other Parts Discussed in Thread: TPS62913
Hello,
I designed a battery charger around the BQ24170 using the BQ2417X calculation tool V1 and filled all the parameters according to my needs (see attached).
The BQ24170 data sheet specifies:
ACOV provides protection to prevent system damage due to high input voltage. In bq2417x, once the voltage on OVPSET is above the 1.6 V ACOV threshold or below the 0.5 V ACUV threshold, charge is disabled and input MOSFETs turn off. The bq2417x provides flexibility to set the input qualification threshold. (Perfect!)
For my application, VIN is 9 VDC, R6 = 100K 1%, R7= 15K 1% and OVP is set for 12.2 Volts for safety (OVP max can't exceed 17.00 Volts which is VIN Max for the next regulator used: TPS62913)
Testing the circuit on my PCB, when VIN = exactly 9.00 VDC, OVPSET pin reaches 1.17 VDC, diode D3 starts to blink and the circuit goes in protection which is unusual regarding the 1.6V ACOV threshold announced above.
Did I something wrong?
So, do you have any explanation regarding this issue and how to solve it?
Thank you,
Kind Regards,
Guy Berwart