Other Parts Discussed in Thread: LM3402, LM3404, LM3404HV
We are powering a string of 6 LEDs with the AN-1839 LM3402/LM3404 Fast Dimming and True Constant LED Current Evaluation Board. SNVA342E-July 2008-Revised April 2013. The strings of 6 LEDs are either yellow, red ,or green and driven from 200ma to 700ma. We need a minimum dimming ratio of 25000 but would prefer 30,000. We are having noise issues and flickering at our lowest intensity settings. The power supply is 28VDC for the Eval board/LEDs. 5VDC for our logic circuits. Jumper 1 on the eval board is closed. Our 4 lowest intensity setting pules are generated by 74HCT123. The PWM frequency is 250Hz generated by a 555 timer. Our lowest pulse widths are 150 nano sec, 330 ns, 660 ns and 1.3 micro sec. These pulse width signals and all the higher intensity signal are sent to a 74HCT4067 and the selected intensity signal is sent to the LM3404 Eval board CONN-1. The 555 timer/hct123 circuit board is hand built with dip chips. The HCT4067 is a surface mount circuit board. The lowest intensity, 150 ns, causes random flickering around 1 or 2 per second and then may be steady for a second or two. Occasionally the 2nd intensity level will cause some flickering.
My questions are;
Can we operate the LM3404 or LM3404HV using MOSFET shunting with this short of a pulse, 150ns, or are we exceeding the specs of the device. Looks to me like it should work. We would like to go down to 100ns.
Should the LM3404 Eval board work with 150 ns pulse(PWM 250Hz).
Are there any circuit changes that you can suggest that would help eliminate the noise. The 150ns pulse looks good (and the other low intensity pulses) until the power is turned on for the LM3404 Eval board.
Thank you for your help