The I2C of the RK3399 cannot communicate with the BQ28Z610 meter successfully if it exceeds 30K Hz. The following is the communication rate of 100K. It can be seen that the ninth ACK bit is a little abnormal, but there is still data returned later, but the data is wrong. The ACK bit is also returned from the battery side, and the data is also returned from the battery side.