This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: RemCap slightly decreased although AvgCurrent shows still 0 (no load)

Guru 29585 points
Part Number: BQ27510-G3
Other Parts Discussed in Thread: BQ27510EVM

Hi Team,

We found RemCap slightly decreased although AvgCurrent always shows 0 (no load) with BQ27510EVM + battery.
RemCap decreased about 1mAh in 30 minutes.
Is it a possible case for BQ27510EVM?

StbyCurrent always shows -2mA.
Is it related to RemCap decreasing?

Best Regards,
Yaita

  • Is there TI member who can support it?
    If you need additional information or has something unclear, please let me know.

    Best Regards,
    Yaita

  • Yaita,

    1) The TI gas gauges when in [REST] mode will rely on the batteries OCV to update its state of charge

    or

    2) if the standby current is -2mA as you say the gauge will still coulomb count this charge. Avg current will report 0 because that is below the default "deadband" current (3mA), but it will still count that charge expelled. 

    Thanks,

    Eric Vos