Hi,
Data sheet states that BQ24297 is compatible with BC1.2.
However, is it compliant in the following situations?
The default setting is D+/D- floating status.
According to Table2,
・If DCD timeout (D+/D- floating), shift to non-standard detection judgment
・If unknown in non-standard detection judgment, set to power supply with default 500mA
With this default setting, if customer use a cable without D+/D- wiring, BQ24297 will not be able to respond correctly.
Could you tell me the stance of BQ24297 when using a cable without D +, D-wiring and ?
Thanks
Yusuke