We have a customer inquiring about the enable pins timing and any limitations for REG71050DDCT,here are the inquiry from the customer in verbatim:
I want to use REG71050DDCT to drive a 5V buzzer with 5V and ~30ma.I was thinking about using the enable pin as a on/off for the this.
Is there a limit to the on/off cycling of the enable pin, or a reason this wouldn't work correctly.
I am looking to add this to my design. I was going to use this IC to get 5V and then use a mosfet to source power from it to the buzzer, but why use another control line if the enable on this IC can do the same thing? I just want to know if there are unforseen reasons to not use this chip this way.
I might have to turn it of and on multiple times over a short period, thought it shouldn't be any quicker than 1 second or so.
There is not much information about the enable pins timing and any limitations it may have turning it off and on allot in a short period of time.
Thank you in advance.