This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ62440-Q1: LMQ62440A-Q1 design to replace LM61435AFS-Q1

Part Number: LMQ62440-Q1

Hi team,

customer would like use LMQ62440A-Q1 to replace the LM61435AFS version since delivery issue.

for LM61435AFS, they select 2.1MHz,

check the LMQ62440A-Q1 d/s, if pin 6 mode/sync pin connect to GND via resistor, it will work in 2.1M/Auto mode/spread spectrum, right?

I have some questions about this

1. for fix 3.3V/5V version of LMQ62440-Q1, how to design FB pin circuit? float or connect to VOUT directly without resistor divider?

2. for LMQ62440-Q1, what's the fsw, is it fixed 2.1MHz or it is adjustable? if it is adjustable, how to adjust? for LM61435, it can be control by RT ?

3. for LMQ61440-Q1, if we want it work in 2.1MHz/FPWM/spread spectrum, how to design pin 6, does it need divider to meet mode_therhold voltage? can you give a reference ciruit?

thank you

  • HI

    LMQ62440 is fixed 2.1Mhz, RT controls the mode of operation of the LMQ62440-Q1. Modes include Auto Mode (automatic PFM / PWM operation), FPWM, and synchronization to an external clock. When synchronized, the clock triggers on rising edge of an external clock. Also, spread spectrum operation is controlled by this pin. 

    1. fixed voltage output, FB connect to Vo

    2.it is fixed 2.1Mhz, for LM61435, fsw can be changed by RT

    3. see datasheet section 8.3.2