This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521855: EVM with AM64xx

Part Number: TPS6521855
Other Parts Discussed in Thread: TPS6521815

Hi

Do you have the plan to release the EVM of TPS6521855 and AM64xx?

I can not find it.

Best Regards,

Kuramochi

  • Kuramochi,

    The Sitara team will be releasing an EVM of the TPS6521815 (DIY-PMIC version of TPS65218xx, programmed to the register settings of TPS6521855) and AM64x. The only reason this EVM uses the TPS6521815 instead of the TPS6521855 is because the TPS6521855 was not available yet. Please find the product page here. As the page indicates, the EVM is currently in the prototype phase and is available in limited quantities. I recommend contacting the Sitara team to be able to get access. I have pinged them on this thread for follow-up.

    Best,
    Emily

  • Hi Kuramochi-san,

    The AM64xx Starter Kit (https://www.ti.com/tool/SK-AM64) uses this PMIC and is available today.

    The bill of materials specifies the TPS6521855.  As Emily stated, early builds are populated with the TPS6521815 that was programmed prior to production, making it equivalent to the TPS6521855.

    Regards,
    Mike